The integration aims to provide an enjoyable travel experience for commuters allowing them to purchase a transport entitlement on their phone without delay, and simply place their phone on the terminal to ride. The Google Pay solution offers rich features such as a map of the transit stations related to their ticket and digital receipts of their travel history.
“At a time when people hail a ride with the push of a button, today’s travelers expect convenience, speed, and trip planning information, no matter how they travel. That’s why we’re so excited about the transformative potential of extending these same benefits to the millions of commuters worldwide who use public transit,” said Pali Bhat, Google’s Vice President of Payments Product Management. “By seamlessly integrating existing MIFARE product based fare payment solutions with Google Pay, transport agencies can provide travelers with a complete digital experience via their mobile devices. We believe this new integration provides a unique opportunity to create powerful new transaction and communication channels between public transit travelers and the systems they depend on.”
With over two billion active users, Android is the largest operating system in the world. Combining Google Pay with the security, flexibility and scalability of MIFARE products, this solution serves as a catalyst for the mobile transit experience, as it will be available for any consumer equipped with widely-available Android phones that support Near-Field Communication (NFC).
“At NXP, our mission is to deliver secure connected solutions that make our lives safer, and more enjoyable. Mobile MIFARE services empower people to benefit from a connected lifestyle by simply connecting devices to a rich set of city services,” said
Scalable and Secure for Transit Agencies
MIFARE 2GO is designed to work with existing MIFARE contactless technology infrastructures and meet industry requirements for security and scalability. Available to transit agencies across the globe, its flexibility and efficiency allow public transport operators to define their fare concepts and provide additional value to their customers by integrating additional city services even if they are from third party providers (such as bike sharing, parking, etc.). Reduced cash handling and credential management costs make MIFARE 2GO an attractive solution for service providers. For more information about the MIFARE 2GO cloud service, please visit www.mifare.net/mifare2go.
NXP and
For mobile devices, Common Criteria EAL5+ SE+NFC solutions from NXP can be used as a high-level security protection enclave. Offering high levels of security allows manufacturers and developers to mitigate the risk of breaches.
First Deployment of MIFARE 2GO with Google Pay in
The first deployment of this solution went live today with the Las Vegas Monorail. The rail system connects hotel resorts and major convention facilities along the Las Vegas Strip and carries a diverse global ridership base, exposing millions of customers annually to this new transit purchasing and information experience. The Monorail has a partnership history with NXP when the companies collaborated to implement the first-ever integration of transit fare into a convention badge during CES 2017.
“We’re so pleased to work with NXP again and introduce yet another global first in the world of transit rider experience and fare integration,” said
NXP Secure Mobile Transit Solutions
Mobile transit enablement is part of NXP’s mission to bring seamless and connected experiences to consumers. It is the only company in the world that can provide a complete end-end solution for a mobile wallet which includes NFC hardware and software, embedded Secure Element hardware, Java Card OS, Applets, Trust Provisioning Services for security, and provisioning services for payment, transit and other applications. Across the world, NXP has several successful smart mobile transit implementations of secure tap-to-pay use cases as well as proven secure, scalable MIFARE deployments.
About
NXP and the NXP logo are trademarks of
For more information, please contact:
Americas | Europe | Greater China / Asia | |||
Tate Tran | Martijn van der Linden | Esther Chang | |||
Tel: +1 408-802-0602 | Tel: +31 6 10914896 | Tel: +886 2 8170 9990 | |||
Email: tate.tran@nxp.com | Email: martijn.van.der.linden@nxp.com | Email: esther.chang@nxp.com |