EINDHOVEN,
JPL has leveraged the high performance and flexibility of NXP’s Layerscape processors in its new 5G NR solutions. The combination enables a powerful offering that has successfully tested at 100 MHz channel bandwidth in 3.5 GHz spectrum with peak data rates of 1 Gbps+. This translates to increased performance for a wide range of segments, enabling innovative applications in smart cities, smart homes, health and education, and significantly enhanced user experience in data download rates for all mobile users. As a result, JPL’s 5G NR radio solutions are well suited for next generation RAN networks, providing increased indoor and outdoor performance and enabling a wide range of 5G use cases.
“The NXP processor platform is an important component of Jio’s 5G journey. 5G New Radio solutions require flexibility in terms of the platform features, efficiency and rich tooling, which NXP brings to the table. Along with NXP, Jio Platforms has developed state-of-the art radio products, which are compliant to the 3GPP as well as to the O-RAN standards. We have a history of close collaboration with NXP, and we look forward to strengthening it further,” said Mr.
NXP’s Layerscape® family of multicore processors provides high levels of integration and deliver strong performance leveraging the combination of Arm 64-bit cores, networking and security offload engines with wide high-speed SerDes interfaces for highly integrated system implementation. Hardware networking offload include switching, timing, parsing and Quality of Service (QoS), providing offload for eCPRI C/U- and S-Plane offload including virtualized and containerized L1/L2 applications. The overall system delivers efficient, scalable performance via software programmable implementation.
“The collaboration with Jio to develop, test and deploy 5G solutions underscores the power of our Layerscape products and the growing ability of NXP’s antenna-to-processor portfolio to accelerate new 5G deployments,” said
NXP’s 5G Access Edge Portfolio
From antenna-to-processor, NXP offers a robust portfolio of technologies for accelerating 5G deployments that delivers best-of-class performance and security for infrastructure, industrial, and automotive applications. This includes the company’s Airfast family of RF power solutions and its Layerscape family of multicore processors for wireless data links, fixed wireless access, and small cell devices. To learn more, visit nxp.com/5G.
About NXP Semiconductors
NXP, the NXP logo and EdgeLock are trademarks of NXP B.V. All other product or service names are the property of their respective owners. All rights reserved. © 2021 NXP B.V.
For more information, please contact:
Jason Deal | |||||
Tel: +44 7715228414 | Tel: +86 21 2205 2690 | ||||
Email: jason.deal@nxp.com | Email: ming.yue@nxp.com |
About
Senior Vice President Tel: + 91 22 244776266 E-Mail: aayush.bhatnagar@ril.com NXP-IoT |
A photo accompanying this announcement is available at https://www.globenewswire.com/NewsRoom/AttachmentNg/40f2c4b8-774a-42b0-aafc-b7117e9d106f
Source: NXP Semiconductors N.V.