MADRID, Spain,
|
The MRFX series of 65 V LDMOS devices targets industrial, scientific and medical (ISM) applications such as laser generation, plasma processing, magnetic-resonance imaging, skin treatment and diathermy, as well as the growing segment of RF Energy where transistors replace vacuum tubes in industrial heating machines. They are also designed for radio and TV broadcast transmitters.
“In less than a year, more than 100 customers have already adopted NXP’s 65 V LDMOS,” said Pierre Piel, senior director and general manager for multi-market RF power at NXP. “Beyond the performance leadership, it is the unprecedented availability of enabling tools that explains this success. Namely, NXP’s power blocks with easy to reproduce designs and available system and software enablement. That means simplified RF design and fast time to market, so our customers can focus on the core value of their products.”
65 V LDMOS made its debut in 2017 with the MRFX1K80H device, capable of 1800 W CW (continuous wave) in an air-cavity ceramic package. Many new reference circuits for the MRFX1K80H have since been designed, enabling RF designers to jump-start their development at 27, 64, 81.36, 87.5-108, 128, 175, 174-230 and 230 megahertz (MHz).
Focusing on ease of use to enable faster development time and design reuse from previous 50 V solutions, NXP recently added to its 65 V offering:
Power supply manufacturers are enabling 65 V solutions.
Availability and Development Support
All 27, 64, 81.36, 87.5-108, 128, 175, 174-230 and 230 MHz reference circuits for the MRFX1K80H are available. The MRFX600H transistor is released, supported by 87.5-108 MHz and 230 MHz reference circuits. The MRFX035H transistor is released, supported by 1.8-54 MHz, 30-512 MHz and 230 MHz reference circuits. For pricing or additional information, please contact your local NXP sales office or NXP approved distributor. All devices of the MRFX series are part of NXP’s 15-year Product Longevity Program.
For more information, visit www.nxp.com/65V.
About NXP Semiconductors
NXP Semiconductors N.V. (NASDAQ:NXPI) enables secure connections and infrastructure for a smarter world, advancing solutions that make lives easier, better and safer. As the world leader in secure connectivity solutions for embedded applications, NXP is driving innovation in the secure connected vehicle, end-to-end security & privacy and smart connected solutions markets. Built on more than 60 years of combined experience and expertise, the company has 30,000 employees in more than 30 countries and posted revenue of $9.26 billion in 2017. Find out more at www.nxp.com.
For more information, please contact:
Americas | Greater China/Asia | Europe |
Tate Tran | Esther Chang | Martijn van der Linden |
Tel: +1 408-802-0602 | Tel: +886 2 8170 9990 | Phone: +31 6 1091 4896 |
Email: tate.tran@nxp.com | Email: esther.chan@nxp.com |
Email: martijn.van.der.linden@nxp.com |
A photo accompanying this announcement is available at http://www.globenewswire.com/NewsRoom/AttachmentNg/18d5b1e3-7283-46f6-b4f5-c957eb55dd65