EINDHOVEN,
New vehicle insurance policies driven by telematics data, which have reached penetration rates as much as 30% in some insurance companies,* represent a market that is expected to grow over 27% annually as insurance providers develop new data-driven insurance products. ** Access to a broader automotive dataset, with more detailed and accurate insights, can enable the development of next-generation analytics tools for actuarial analysis, new mobility product development and claims management.
While connected vehicles can generate terabytes of data per hour, some of which can be leveraged for sophisticated underwriting and multiple business applications, carmakers and insurance companies are impeded from a lack of available, cost-effective data processing platforms with sufficient performance, security and centralized access to vehicle-wide data.
To meet this need, NXP and MOTER have integrated their offerings into a platform that targets the needs of the automotive and insurance industries. The MOTER platform offers advanced risk algorithms that can be updated over-the-air and combined with an insurance carrier’s or mobility company’s custom insurance algorithms to create marketable driver insights. The MOTER platform can be licensed for use with OEM vehicles to facilitate data exchange with insurers and mobility companies who are willing to subscribe and pay for driver insights to enable new vehicle data-driven products, including, but not limited to, usage-based insurance.
“Usage-based insurance is one of the data commercialization opportunities with the most customer satisfaction and revenue potential for the automotive industry today,” said
NXP’s GoldBox reference design, based on one of the recently launched S32G2 vehicle network processors, is a key enabler for new vehicle data-driven opportunities such as advanced insurance, vehicle health and fleet management services. It provides safe and secure vehicle edge processing, support for Over-the-Air (OTA) services, and connectivity to in-vehicle networks and the cloud required for these next-generation automotive applications. S32G2 processors provide both high-performance real-time and applications processing combined with vehicle network interfaces, network acceleration and hardware security, along with expansion support for machine learning (ML) acceleration, mass storage and wireless connectivity to deliver a powerful service-oriented gateway.
“Vehicle data will power new automotive business opportunities in the near future, similar to the apps proliferation and big data insights provided by the smartphone over the past decade,” said
To find out more about the collaboration between MOTER and NXP visit https://moter.ai/nxp-moter
* Source: Novarica - Oct' 20
** Source: MarketsandMarkets – June “21
About NXP Semiconductors
NXP and the NXP logo are trademarks of NXP B.V. All other product or service names are the property of their respective owners. All rights reserved. © 2021 NXP B.V.
About
MOTER Technologies is a software and data science company focused on bridging the gap between the automotive and insurance ecosystems. The insurtech company continues research and development begun within its parent organization, with a focus on commercialization of connected car data and development of new insurance products and services in collaboration with OEMs, Tier 1s, insurance companies and new mobility fleets. http://www.moter.ai
For more information, please contact:
Americas & Europe | Greater China / Asia | |
Tel: +44 7715228414 | Tel: +86 21 2205 2690 | |
Email: jason.deal@nxp.com | Email: ming.yue@nxp.com |
NXP-Auto
A photo accompanying this announcement is available at https://www.globenewswire.com/NewsRoom/AttachmentNg/11c3dfea-b2ed-4888-ad87-b4f2422b7fb7
Source: NXP Semiconductors N.V.