EINDHOVEN,The Netherlands,
|
Additionally, NXP announced that it has been working with Arm as the lead technology partner in evolving Arm® Ethos-U™ microNPU (Neural Processing Unit) architecture to support applications processors. NXP will integrate the Ethos-U65 microNPU into its next generation of i.MX applications processors to deliver energy-efficient, cost-effective ML solutions for the fast-growing Industrial and IoT Edge.
“NXP’s scalable applications processors deliver an efficient product platform and a broad ecosystem for our customers to quickly deliver innovative systems,” said
Enabling Machine Learning for All
Au-Zone’s DeepView™ ML Tool Suite will augment eIQ with an intuitive, graphical user interface (GUI) and workflow, enabling developers of all experience levels to import datasets and models, rapidly train, and deploy NN models and ML workloads across the NXP Edge processing portfolio. To meet the demanding requirements of today’s industrial and IoT applications, NXP’s eIQ-DeepViewML Tool Suite will provide developers with advanced features to prune, quantize, validate, and deploy public or proprietary NN models on NXP devices. It’s on-target, graph-level profiling capability will provide developers with unique, run-time insights to optimize NN model architectures, system parameters, and run-time performance. By adding Au-Zone’s DeepView run-time inference engine to complement open source inference technologies in NXP eIQ, users will be able to quickly deploy and evaluate ML workloads and performance across NXP devices with minimal effort. A key feature of this run-time inference engine is that it optimizes the system memory usage and data movement uniquely for each SoC architecture.
“Au-Zone is incredibly excited to announce this investment and strategic partnership with NXP, especially with its exciting roadmap for additional ML accelerated devices,” said
Expanding Machine Learning Acceleration
To accelerate machine learning in a wider range of Edge applications, NXP will expand its popular i.MX applications processors for the Industrial and IoT Edge with the integration of the Arm Ethos-U65 microNPU, complementing the previously announced i.MX 8M Plus applications processor with integrated NPU. The NXP and Arm technology partnership focused on defining the system-level aspects of this microNPU which supports up to 1 TOPS (512 parallel multiply-accumulate operations at 1GHz). The Ethos-U65 maintains the MCU-class power efficiency of the Ethos-U55 while extending its applicability to higher performance Cortex-A-based system-on-chip (SoC)s. The Ethos-U65 microNPU works in concert with the Cortex-M core already present in NXP’s i.MX families of heterogeneous SoCs, resulting in improved efficiency.
“There has been a surge of AI and ML across industrial and IoT applications driving demand for more on-device ML capabilities,” said
Availability
Arm Ethos-U65 will be available in future NXP’s i.MX applications processors. The eIQ-DeepViewML Tool Suite and DeepView run-time inference engine, integrated into eIQ, will be available Q1, 2021. The end-to-end software enablement, from training, validating and deploying existing or new neural network models for i.MX 8M Plus and other NXP SoCs, as well as future devices integrating the Ethos-U55 and U65, will be accessible through NXP’s eIQ Machine Learning software development environment. To learn more read our blog and register for the joint NXP and Arm webinar on
About
NXP, the NXP logo and EdgeVerse are trademarks of
For more information, please contact:
Jason Deal | |||||
Tel: +44 7715228414 | Tel: +86 21 2205 2690 | ||||
Email: jason.deal@nxp.com | Email: ming.yue@nxp.com |
NXP-IoT
NXP-Smart Home
NXP-Corp
A photo accompanying this announcement is available at https://www.globenewswire.com/NewsRoom/AttachmentNg/ea5038f6-c957-4d81-866f-e613cbe439f6
Source: NXP USA, Inc.