Solution enables new intelligent & secure services in the home, and simplified on-the-fly deployment
|
BERLIN,
Edge Computing technology aims to harness the power of cloud computing and artificial intelligence while addressing the need for low latency, privacy and reliability of many use-cases. For example, an application such as face recognition for a “video doorbell” can run the machine-learning in the cloud and download the inference model to the Home Gateway at set intervals. This means that camera data does not need to continuously stream to the cloud, and the application continues to work even when an internet connection is lost. NXP’s EdgeScale technology for secure onboarding and management of IoT devices covers the entire dataflow from edge to cloud.
The edge solution’s approach has several advantages over traditional application software architectures including the ability to dynamically deploy without rebooting. It can also securely separate applications from critical services and leverage both cloud and edge computing power, including artificial intelligence. The most significant innovation is that the same run-time environment is available on both the cloud and the edge device (Home Gateway in this case) – so that developers can write new applications without deep knowledge of the embedded system.
“Combining SoftAtHome’s modular gateway platform with NXP’s EdgeScale technology and high-performance multi-core processors will accelerate the availability of a new computing model for the home,” commented Noy Kucuk, vice president, digital networking at NXP. “We are excited to be working with SoftAtHome to deliver new services based on artificial intelligence in the hybrid cloud-edge.”
“SoftAtHome provides a robust home network software product with great Quality of Service. Connect’ON transforms operator-Home Gateways into high-performance secure service delivery platforms and can support the needed technologies to provide best-in-class broadband services, including Edge computing,” added Lionel Gremeau, marketing product director, SoftAtHome. “Our cooperation with NXP will accelerate the adoption of this new paradigm.”
NXP and SoftAtHome will demonstrate the programmable platform to invited customers during the
About NXP Semiconductors
About SoftAtHome
SoftAtHome creates software for operators to deploy services with the best user experience for connectivity, pay TV, Home Networking and Smart Home products. SoftAtHome products are deployed with major operators in over 20 million homes over 18 countries. The company based in France and Belgium is still growing with over 250 employees mainly in software development. We are regularly opening new offices to support our customers. Offices are already in half a dozen European capitals as well as in Dubai, Singapore and Toronto. More info: www.softathome.com
The NXP logo and Layerscape are trademarks of
For more information, please contact:
NXP Europe
Martijn van der Linden
Phone: +31 6 1091 4896
Email:
martijn.van.der.linden@nxp.com
NXP Americas
Jacey Zuniga
Phone: +1 512-895-7398
Email:
jacey.zuniga@nxp.com
SoftAtHome
Marta Twardowska for SoftAtHome
E: press@softathome.com
M: +31 621-184-585