PHILADELPHIA,
|
mMIMO is an essential foundation for 5G, as it answers the network’s need for a radio frequency (RF) technology capable of handling the huge increase in data usage that 5G is expected to bring. mMIMO meets that challenge by enabling the transmission of far more data over a given frequency spectrum than any current, traditional radio technologies allow.
NXP’s new Front-End Solutions for 5G, unveiled at this week’s International Microwave Symposium (IMS2018), address the significant, critical challenge of creating cost-effective, high performance solutions in the smallest form factor to enable the next generation of active antenna systems (AAS) for cellular infrastructure. Or, to put it more simply: so that everything needed for mMIMO can fit into the smallest box possible.
NXP answers that challenge with a portfolio of highly integrated solutions that feature much smaller form-factors— making them easy and more cost-effective for customers to plug-and-play between all frequency bands and power levels. “These devices have been developed to enable our customers to design their systems at the lowest cost possible,” says Mario Bokatius, product line director for NXP’s front-end solutions.
The NXP front-end solutions cover the frequency range most critical for early 5G cellular network development, from 2.3 GHz to 5 GHz.
NXP Front-End Solutions for 5G Enablement consist of three different functions critical to creating an RF front-end for mMIMO:
“We offer the highest levels of integration without compromising high performance requirements – but this is just the beginning,” says Bokatius. “Moving forward, you can look to NXP for even more integration as we continue our commitment to providing the industry’s smallest footprint and lowest cost solutions.”
NXP leveraged its silicon LDMOS technology to enable the most favorable cost structure for its RF customers. LDMOS has undergone continuous innovation since its introduction decades ago. The ability of LDMOS to consistently deliver ever-increasing levels of high power, with high gain and efficiency, along with its remarkable ruggedness and low heat characteristics, has made it the dominant device technology in RF power amplifier applications from below 1 GHz to 3 GHz. NXP’s LDMOS technology is now extending that leadership into the frequency range up to 5 GHz. LDMOS allows these solutions to deliver high performance, comparable to the performance of non-silicon RF power transistors but with greater reliability and at lower cost.
“Our leadership and deep wireless communication industry knowledge positions us well to be an instrumental partner to continue delivering 5G solutions for our customers,” says Paul Hart, senior vice president and general manager of NXP’s
Availability
The majority of
To learn more, visit NXP at IMS2018, booth #739 or at www.nxp.com/RF.
About NXP Semiconductors
NXP Semiconductors N.V. (NASDAQ:NXPI) enables secure connections and infrastructure for a smarter world, advancing solutions that make lives easier, better and safer. As the world leader in secure connectivity solutions for embedded applications, NXP is driving innovation in the secure connected vehicle, end-to-end security & privacy and smart connected solutions markets. Built on more than 60 years of combined experience and expertise, the company has over 30,000 employees in more than 30 countries and posted revenue of $9.26 billion in 2017. Find out more at www.nxp.com.
For more information, please contact: | ||
Americas | Europe | Greater China / Asia |
Jacey Zuniga Tel: +1 512-895-7398 Email: jacey.zuniga@nxp.com |
Martijn van der Linden Tel: +31 6 10914896 Email: martijn.van.der.linden@nxp.com |
Esther Chang Tel: +886 2 8170 9990 Email: esther.chang@nxp.com |
Photos accompanying this announcement are available at
http://www.globenewswire.com/NewsRoom/AttachmentNg/c4992f59-9e8b-42ef-ae4e-1b69ff800778
http://www.globenewswire.com/NewsRoom/AttachmentNg/79628af1-32c7-42a6-b979-1655860a004a