Press Release

NXP GreenBox Development Platform Accelerates Transition to Hybrid and Electric Vehicles (HEVs/EVs)  

February 20, 2018 at 2:01 AM EST
High-performance processing platform used to design and test control algorithms and energy management tasks for next-generation electric drive vehicles

NUREMBERG, Germany, Feb. 20, 2018 (GLOBE NEWSWIRE) -- NXP Semiconductors N.V. (NASDAQ:NXPI), has announced the availability of its GreenBox vehicle electrification development platform. GreenBox allows automakers and suppliers to begin early development of next-generation hybrid and electric vehicle applications on NXP’s S32 automotive processing multicore platform based on Arm Cortex technology.

With increasing regulatory restrictions on emissions and stricter fuel economy targets around the world, both traditional automakers and new market entrants are under pressure to roll out electric and hybrid vehicles to consumers quickly. GreenBox provides a high-performance processing platform to design and test new control algorithms and energy management tasks critical for next-generation hybrid and fully-electric vehicles.

GreenBox is one of the development platforms for NXP’s next generation S32 electrification MCUs, which are part of the S32 automotive processing platform that is built around a safe, secure and fault-tolerant configuration. The S32 electrification MCUs will address the increasingly intensive computation and memory requirements for tomorrow’s HEV/EV applications.

Using the GreenBox development environment, developers can also tap into the mix of high-performance and highly optimized peripherals, including advanced timers, motor control peripherals and analog sub-systems to interface with their own development hardware.

GreenBox is available in two configurations. The first is for development of fully-electric vehicles and supports motor control and battery management capabilities. The second is for development of hybrid applications, which supports both electric vehicle features as well as traditional engine control capabilities.

Recently, China, India, France, several states within the U.S. and other countries have either passed laws on internal combustion engine production termination or have signaled legislative intentions. Furthermore, the compounded annual growth rate for internal combustion engines is in decline as hybrid and electric are growing.

“The combination of regulatory and market indicators as well as long automotive development cycles require automakers to begin the development of HEV/EV systems now -- before the next wave of processors for electrification are available,” Ray Cornyn, vice president of Vehicle Dynamics and Safety said. “GreenBox meets this challenge by providing automakers a hardware development environment before the NXP S32 electrification MCU is available.”

About the GreenBox Vehicle Electrification Development Platform

  • Aimed at hybrid, electric and internal combustion propulsion, including traction motors, motor control units, battery management systems, hybrid/vehicle control units and integrated DC/DC converters
  • Hardware development board with Arm Cortex-based development environment
  • Peripheral board optimized for either Hybrid/internal combustion or motor control/battery management applications 
  • Includes AUTOSAR operating system and MCAL drivers
  • Developers have access to S32 Design Studio IDE
  • Simple out-of-the box experience includes a Quick Start Guide and application code with basic control examples

NXP GreenBox at Embedded World 2018
NXP Green Box development platform will demo the performance capabilities of next-gen MCUs as they manage both the electric motor and internal combustion engine applications for the hybrid electric vehicles of tomorrow.

NXP GreenBox Is Now Available
GreenBox electrification development platform is available today in limited quantities to Alpha customers. Contact your sales person for more information.

More at www.nxp.com/GreenBox

About NXP Semiconductors

NXP Semiconductors N.V. (NASDAQ:NXPI) enables secure connections and infrastructure for a smarter world, advancing solutions that make lives easier, better and safer. As the world leader in secure connectivity solutions for embedded applications, NXP is driving innovation in the secure connected vehicle, end-to-end security & privacy and smart connected solutions markets. Built on more than 60 years of combined experience and expertise, the company has over 30,000 employees in more than 30 countries and posted revenue of $9.26 billion in 2017. Find out more at www.nxp.com

For more information, please contact:

Europe / U.S.
Jason Deal
Tel: +44 7715228414
Email: jason.deal@nxp.com

Greater China / Asia
Esther Chang
Tel: +866 2 8170 9990
Email: esther.chang@nxp.com

Japan
Kiyomi Masuda (増田 清美)
Tel: +81-70-3627-6472
Email: kiyomi.masuda@nxp.com

Primary Logo

NXP USA, Inc.