EINDHOVEN, The Netherlands,
|
Echo and noise can make communication on the road difficult. Echo occurs when the speakers within a car transmit a voice signal from an incoming call, which subsequently ricochets through the vehicle and returns to the microphone. This causes the caller to hear their own voice, which is distracting and can result in broken communications. Additionally, road noise from fans, exhaust, tires, windows and passengers can infiltrate calls and render them unintelligible, ultimately disrupting the driving experience and causing frustration.
The new NXP ECNR solution deals with both problems by removing echoes and filtering out unwanted noise from the cockpit to enhance the sound quality of conversations. Since the ECNR solution can be ported to NXP chipsets and is ITU-T P1110 and CarPlay® pre-certified, it can reduce carmakers’ R&D expenses and speed up the design cycle.
Quote:
“The NXP ECNR software has been deployed worldwide in more than a billion phones 2 and we want to deliver this leading3 market-proven technology to our automotive customers,” said Alexandre Henon, marketing director of audio solutions at NXP. “We adapted our ECNR to automotive requirements and ported the software on two NXP chipset families to provide NXP customers with an easy to implement, high-performance and architecturally flexible solution depending on where they want to run the ECNR function.”
Availability
The ECNR algorithm is running on the HiFi2 core of SAF775x, ready be activated by a key code.
Notes
1 Source - Strategy Analytics 2016
2 Source - Based on internal data
3 Source – SAR Insight & Consulting
About NXP Semiconductors
For more information, please contact:
Europe / U.S.
Jason Deal
Tel: +44 7715228414
Email: jason.deal@nxp.com
Greater China / Asia
Esther Chang
Tel: +866 2 8170 9990
Email: esther.chang@nxp.com
Japan
Kiyomi Masuda (増田 清美)
Tel: +81-70-3627-6472
Email: kiyomi.masuda@nxp.com
A photo accompanying this announcement is available at http://www.globenewswire.com/NewsRoom/AttachmentNg/aa5e8f6d-1946-4c21-8903-34e37b458e87