Financial Press Releases

NXP Enables Service-Oriented Gateways for Automakers to Unlock Value of Connected Vehicle Data
Automotive-grade chipset revolutionizes vehicle gateways with secure applications processing and network acceleration

NUREMBERG, Germany, Feb. 26, 2019 (GLOBE NEWSWIRE) -- (Embedded World 2019) – NXP Semiconductors N.V. (NASDAQ: NXPI), the world’s largest supplier of automotive semiconductors1, today announced a vehicle network processing chipset solution for high-performance service-oriented gateways, which enables automakers to unlock the value of connected vehicle data and offer new services. The MPC-LS chipset solution combines the proven NXP automotive MPC5748G microcontroller and enterprise networking LS1043A communications processor to offer the high levels of performance and networking required for service-oriented gateways. For development, evaluation and demonstrations, the chipset solution is supported by an evaluation board, enablement software and a growing ecosystem.

Vehicle data-driven services such as usage-based insurance, predictive maintenance and over-the-air upgradeable vehicles are projected to reach up to $750 billion in revenue by 20302. These services and the information derived from connected vehicles are poised to transform the automotive industry with new revenue opportunities, improved user experiences, safety and security enhancements and cost reductions. To enable these new opportunities, centrally located service-oriented gateways must securely process and route massive amounts of data across the vehicle, which requires a vehicle network processing solution to meet the demand.

NXP helps automakers, suppliers and emerging global entrants develop new vehicle networking platforms of the future today. The production-ready MPC-LS vehicle network processing chipset  uniquely brings together real-time and applications processing, along with automotive and enterprise networking technologies.

Key features include:

  • High-performance quad-core, 64-bit Arm® processors for services and edge analytics
  • One 10 Gigabit and five Gigabit Ethernet interfaces for high-bandwidth networking
  • Ethernet packet acceleration offloads processors to provide valued services
  • Real-time processing of vehicle data from CAN FD, LIN and FlexRay™ networks
  • Hardware security for trusted boot, cryptography and secure key management

A connected vehicle can generate terabytes of data daily from sensors, vehicle usage, and driver and passenger behaviors. A service-oriented gateway has the performance to conserve wireless network bandwidth by converting raw data into actionable information that can be sent to the cloud for additional analysis and storage with reduced cost.

“The powerful combination of automotive and enterprise network processing technology provided by the MPC-LS chipset for development of vehicle gateways can enable a new era of vehicle services and edge processing,” said Jake Alamat, vice president of Automotive Connectivity and Security at NXP. “The value of the solution has been well-received by automakers and is scheduled to be deployed in volume vehicle production starting in 2020.”

AVAILABLE NOW

The automotive-qualified MPC-LS vehicle network processing chipset, comprised of the MPC5748G microcontroller and LS1043A communications processor, is available today.

An evaluation board (MPC-LS-VNP-EVB), with enablement software support for bare metal, and AUTOSAR® and Linux® operating systems to support development, evaluation, and demonstrations, is available in limited quantities. Contact your salesperson for more information.

More information is available at www.nxp.com/VNP

VEHICLE NETWORK DEMOS AT EMBEDDED WORLD 2019

Airbiquity is a partner in the growing MPC-LS ecosystem which will offer new services to carmakers. NXP will demonstrate the MPC-LS VNP Evaluation Board (EVB) integrated with Airbiquity’s OTAmaticTM over-the-air (OTA) software and data management services at embedded world 2019.

“NXP’s MPC-LS chipset enables Airbiquity’s OTAmatic™ OTA software and data management solution to offer advanced features requested by carmakers with the capacity to support future services,” said Keefe Leung, director of product management for Airbiquity, a service provider in the growing ecosystem. “The ability to run multiple concurrent edge analytics modules while providing secure OTA updates over multiple vehicle network interfaces creates new opportunities for our customers.”

NOTES

1 Source: Strategy Analytics, 2017

2 Source: McKinsey & Company, Monetizing Car Data, 2016

About NXP Semiconductors

NXP Semiconductors N.V. (NASDAQ:NXPI) enables secure connections and infrastructure for a smarter world, advancing solutions that make lives easier, better and safer. As the world leader in secure connectivity solutions for embedded applications, NXP is driving innovation in the secure connected vehicle, end-to-end security & privacy and smart connected solutions markets. Built on more than 60 years of combined experience and expertise, the company has over 30,000 employees in more than 30 countries and posted revenue of $9.26 billion in 2017. Find out more at www.nxp.com

NXP and the NXP logo are trademarks of NXP B.V. All other product or service names are the property of their respective owners. Arm is a trademark or registered trademark of Arm Limited (or its subsidiaries) in the US and/or elsewhere. The related technology may be protected by any or all of patents, copyrights, designs and trade secrets. All rights reserved.  © 2019 NXP B.V.

For more information, please contact:

NXP

Europe / U.S.
Jason Deal
Tel: +44 7715228414
Email: jason.deal@nxp.com

NXPJPEGLOGO.jpg

NXP USA, Inc.